12/2/2009 5:08 PM | |
Joined: 9/27/2006 Last visit: 7/7/2024 Posts: 12268 Rating:
|
Hello amit_86; Maybe the sequence proposed by uel123 in the following link can help you out clear the matter out: /tf/WW/en/Posts/13246 Hope this helps, Daniel Chartier |
12/5/2009 8:20 PM | |
Joined: 1/29/2006 Last visit: 6/30/2024 Posts: 446 Rating:
|
Hey, amit_86! I am sending you a example of my code for communication with ATLAS-COPCO through Combox-P gateway. In my case, I am reading 6 parameters (=actual values) from 2 compressors. You can easilly expand this to more compressors. But first, please read the post on link, which was sent to you from Daniel Chartier. And also, additionally: 1. Combox must first be properly programmed (I believe, by Atlas Copco people). The telegram lenght must be properly set on COMBOX side. See the telegram lenght from my example, in HW config. 2. At the time, when I was dealing with this problem (in year 2007), I could not find a GSD file for Combox anywhere. Therefore, I have written it for myself, according to instruction from manual for Combox, that was available at the time.As you will see in my project, I could not establish a greater consistency then 1 byteand I am not using SFC14/15. If you manage to work with another GSD file (and establishbigger consistency!), then simple replace NW 21 and 22 in FB 510 withSFC14/15. Have fun! uel123 AttachmentAtlas_co.zip (3368 Downloads) |
This contribution was helpful to
3 thankful Users |
12/14/2009 6:39 PM | |
Joined: 1/29/2006 Last visit: 6/30/2024 Posts: 446 Rating:
|
Hey, Amit! Any success with Combox-p and Atlas copco? have fun! uel123 |
Follow us on