11/13/2023 7:53 AM | |
Joined: 7/11/2014 Last visit: 6/27/2025 Posts: 21 Rating:
|
May be in TIA V19? In page 19 you can find Data types with named values based on IEC 61131-3 [snip] I hope so, even if I do not understand why it is in relationship only with software units... It will be the possibility to use outside software units? It will be possible use it inside an FC or FB as a local variable? AttachmentinfoPLC_net_1699522151434 (1).pdf (317 Downloads) |
Last edited by: qualbuonbomb at: 11/13/2023 08:09:53Last edited by: Jen_Moderator at: 11/13/2023 08:19:17Link removed and file attached. |
|
This contribution was helpful to
1 thankful Users |
11/13/2023 8:12 AM | |
Joined: 3/30/2020 Last visit: 9/11/2025 Posts: 5443 Rating:
|
Only available within software units. That translates also to only S7-1500 based controllers. Page 19 of the document you mention is attached. Attachmentunofficial - TIAP V19 - date types with named values.pdf (332 Downloads) |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on