2/22/2016 2:10 PM | |
Joined: 5/12/2006 Last visit: 7/22/2024 Posts: 22318 Rating:
|
Hello, no the IM Package doesn't contains a U connector, the U Connector is in the Package of the I/O Module. normaly you must not order the connector seperat, use the connector from the I/O module. There is no mechanic in the connector, easy Plug not more. PS or PM ? PS -> yes here you need a U connector PM -> here you need no U connector. But why you don't read the manuals? many of the questions are answered in the manual: https://support.industry.siemens.com/cs/de/en/view/86140384 Regards Christoph |
Last edited by: ChristophD at: 2/22/2016 2:14:25 PMLast edited by: ChristophD at: 2/22/2016 2:15:35 PM |
|
This contribution was helpful to
2 thankful Users |
2/22/2016 6:33 PM | |
Joined: 9/27/2006 Last visit: 7/22/2024 Posts: 12270 Rating:
|
Hello Automoto; Please do not react as if any of us here is trying to confuse you. Every information provided (specially links to documents that you might search in for your own edification) have been very adequate and correct. Now, I believe your reaction comes from a very basic misunderstanding. You seem to believe that since both the S7-300/ET 200M and the S7-1500/ET 200MP both use "U connectors" as backplane communication bus support, that the technology must be the same. But the S76-1500 is 15 years younger that the S7-300 platform, the basic components have evolved between the two platforms. The MLFB for the S7-1500 U connector (can be found in the S7-1500 system manual, for example) ; U connector (spare part), 5 units 6ES7590-0AA00-0AA0 This is the Industry Mall corresponding to this module: https://mall.industry.siemens.com/mall/en/WW/Catalog/Product/6ES7590-0AA00-0AA0 A screenshot is attached. And one U connector is provided for every IO module delivered from the S7-1500 catalog, as has been stated earlier. I hope this closes the issue. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 2/22/2016 10:18:56 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on