8/8/2022 2:54 PM | |
Joined: 9/27/2006 Last visit: 6/27/2024 Posts: 12264 Rating:
|
Hello davdanipr; The 151-8 CPU should have been delivered with a terminating module. https://support.industry.siemens.com/cs/ca/en/view/47409312/19518399883 If it is not properly installed, you will not be able to reach your I/O modules. Can you check whether this is your problem? Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
8/8/2022 3:33 PM | |
Joined: 9/1/2021 Last visit: 8/10/2022 Posts: 20 Rating:
|
Hello, thank you, yes my colleague forgot to install it.. I’ve done it, but still not working. Do you have any idea? |
Last edited by: davdanipr at: 08/08/2022 15:34:34 |
|
8/8/2022 9:54 PM | |
Joined: 9/21/2012 Last visit: 6/28/2024 Posts: 3980 Rating:
|
Looks like you might have a problem with the MLFB number and/or version of the module in the HW compared to real hardware. You can see the problem from the PLC diagnostics buffer. |
8/9/2022 9:14 AM | |
Joined: 9/1/2021 Last visit: 8/10/2022 Posts: 20 Rating:
|
Hello Hati, thank you for your answer. They seems to me OK. Can the firmware version difference a problem? Or should I set something on these rotary knobs (attachment)? That program is a “Standard Program” from our side and that worked already a few times. The Module socket is coming automatically with the ET modules when I adding them to the device config right? Because I don’t know how could I change them.
|
8/9/2022 11:40 AM | |
Joined: 9/1/2021 Last visit: 8/10/2022 Posts: 20 Rating:
|
Hello Duris_l 1: you can find it in Attachment 2: i don’t understand quite understand what do you mean. There is a P1R P2R and P3 ports. 3: Which version do you mesn? Firmware? In TIA i cannot find any infos about it, i think because they are “not reachable”. Yeah you see it right and that was strange to me too that fourth module the SF is not lighting, but in TIA they are also in fault. The errors are the same for all of the modules. +1: No, there is 3 IO-link modules after the DC24V module.
AttachmentDiagnostics.txt (451 Downloads) |
Follow us on