7/12/2009 2:30 PM | |
Joined: 10/7/2005 Last visit: 9/10/2025 Posts: 3049 Rating:
|
Excellent point Phantom75 and the same can be said for the following words from lalit:
Let's also not forget that people tend to like what they know (or have experience with). A/B PLC’s and their programming software are perceived by A/B fans to be “easier”, “more powerful” and more “user friendly” than Siemens PLC’s and I can see where this (WRONG) perception comes from. For one, ControlLogix PLC’s have a wealth of inbuilt instructions (e.g. Array (file) shift/compare/search/sort instructions, FIFO buffer handling, the hideous “compute” instruction etc.etc.) which far exceeds what you’ll find in the “normal” Step7 instruction set. There is of course a wealth of SFC’s/SFB’s available to begin with and a considerable amount of IEC blocks, knowing that they exist can of course be a challenge. I don’t mean to be sarcastic here and its good that these questions are asked, but even in this forum we have questions like “Is there a way to set all values to zero in a DB”, the simple answer is of course “Yes, have a look at SFC21”, but people simple aren't "naturally" aware of these. And you can of course always develop your own blocks to do what you want to do and neatly put them into libraries (or use blocks created by others such as www.oscat.de). Secondly, programming of a ControlLogix PLC takes a lot of the thinking effort away from you. For example, essentially all math and compare instructions exist only as one instruction, whereas Step7 has as set of INT, DINT and REAL for these. And yes, you can compare an INT with a REAL via the A/B compare instruction (you can even compare STRINGS with the same instruction!). The compiler will in runtime convert and match the data types and spit out the result. You can also for example add an INT with a DINT and have the result delivered as a REAL (in one common ADD instruction). People (who don’t know better) like this nonsense, it does however lead to “sloppy” programming techniques and can cause unforeseen results (note that even the manual actually states that every instruction has so called “optimal” data types which makes the instruction execute faster and requires less memory and these are typically DINT or REAL. There is additionally a long section at the end in the instruction set manual that describes what rules govern the conversion of one data type to another if mixed data types are used). Anyway, I’ve seen a colleague during commissioning scratching his head why his comparison didn’t deliver the results he thought it should, until he realised that he fell prey to the usage of mixed data types. To sum this yet again way to drawn out entry up: Siemens PLC’s are more logical, more strictand don’t hide anything from you. Human nature unfortunately favors being a bit lazy and being able to quickly program something without the need to fully understand what you are doing and in this case (and this case alone)A/B programming wins against Siemens programming (and for the record, A/B PLC’s are Toys, I am after all entitled to my narrow-minded point of view Lastely dear lalit, there are twomore points to add to your main list, which are: 1.)Controllogix PLC's don't have a process image available. If you want to ensure that Inputs stay the same throughout the scan you need to create an input buffer via programming. 2.) NO STL available in A/B PLC's (and if this not the clear winner than I don't know what is, I can't belive I didn't think of this straight away) Keep up the good work guys |
Last edited by: fritz at: 7/12/2009 2:54 PMLast edited by: fritz at: 7/12/2009 2:38 PMLast edited by: fritz at: 7/12/2009 2:37 PMCheers |
|
This contribution was helpful to
4 thankful Users |
7/14/2009 7:40 AM | |
Joined: 12/20/2008 Last visit: 9/3/2025 Posts: 556 Rating:
|
Hi Fritz, I can't stop myself from keep giving you 5 Star rating for the efforts you have done to explain this thing so much clearly. Fritz> It is really the people like you and Phantom who makes the things different. You guys are the real expert on this forum, I hope our moderator will recoginze your efforts to keep this forum so lively, so interesting, so much knowledgeable and so much active. Keep it up Guys! And Fritz the below word is absolutely from you. Cheers! |
This contribution was helpful to
4 thankful Users |
Follow us on