4/28/2008 7:45 AM | |
Joined: 9/20/2006 Last visit: 8/1/2025 Posts: 307 Rating:
|
The value of P071 is correctly programmed. |
5/4/2017 4:34 PM | |
Posts: 2 Rating:
|
DEAR. Solución de la alarma F006. Se cambio el encoder que esta acoplado al eje del motor del inversor instalado en el bus DC. Este ocasiona, que se interprete como una detención del motor por lo que ocasiona que el equipo regenere. No existían alarmas en los equipos re-generativos. Nota: Archivo adjunto, equipos instalados ------------------------------------------------------------------------------------------------- DEAR. Alarm solution F006. The encoder that is coupled to the motor axis of the inverter installed on the DC bus is changed. This causes it to be interpreted as an engine stoppage causing the equipment to regenerate.
Note: Attachment, installed equipment AttachmentSolucion F06 Siemens.doc (762 Downloads) |
Last edited by: Min_Moderator at: 5/5/2017 2:22:48 PMtranslation |
|
This contribution was helpful to
1 thankful Users |
5/29/2017 7:52 PM | |
Joined: 9/27/2006 Last visit: 9/5/2025 Posts: 12398 Rating:
|
Hello Junior; I do not know if these were the items you already checked, but let's start with the definition of f006 from the Compendium: https://cache.industry.siemens.com/dl/files/629/109736629/att_880959/v1/vc34_kompend_e.pdf Hope ths helps, Daniel Chartier |
5/30/2017 12:37 PM | |
Posts: 3 Rating:
|
Hello'daniel Regarding the alarm F006 already the parameters in question were verified. This inverter has already run a period of 7 years without problems. The company that works produces for another company, only that this company can modify the machine according to what will be deelvolved of product. They modified the pulley moved of this machine, and after this change the machine began to give the alarm F006 depending on the product to be made. I ask: Does the machine manufacturer put some variable tied to the supervisor and CLP?
|
Follow us on