11/28/2024 12:47 PM | |
Joined: 10/17/2007 Last visit: 9/12/2025 Posts: 4449 Rating:
|
You are talking about to branches--SMODRIVE and SINUMERIK #1--you have SIMODRIVE 611A , and power supply module any type you can use without problem --if they are good functional. 611A is easy to test --I will send you a manual . basically you can use battery box (suggest 1.5 VDC) to terminals 56/14 and enable 633,65, the axis should running #2--CNC 810M, if you load good back up, ( I think I told you ) you have problem for "FEED disable"--RED LED on the 810M front panel on, --it needs PLC program troubleshooting why axis "enable " signal not coming --such as machine hit limit switch , or you machine hydraulic system not working? Attachment57453743611A_IA.pdf (378 Downloads) |
Last edited by: nulizhang at: 11/28/2024 13:11:33If you like my comments please |
|
Follow us on