9/4/2008 9:01 AM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hi Pasant, First off all thanks for the feedback and I'm glad to hear it's functioning now. As EDR told there is a change that bluetooth will affect it. But only real active devices. Like a Bluetooth AP or Mobile Phones which are communicating over the system. But why don't you use 5 GHz, the devices are all capable of doing this you just need the correct antenna. And important to know is or it's allowed in your country. To check or it's allowed you just need to do the following: 1. Your devices needs to be equipped with the newest firmware to get the newest list. Download zum Firmware Update SCALANCE W-700: Download zum Firmwareupdate V3.4.04 2. If the devices is up to date you just type in a web-browser: https://<IP-Adresse des SCALANCE W-700>/countrylist.log 3. in the list you will found information about released channels for the released countries and also or it's available indoor and/or outdoor and with which transmit power. |
Best regards, |
|
10/6/2008 2:47 PM | |
Posts: 10 Rating: (0) |
cole? |
10/6/2008 3:02 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating: (56) |
Hi Pasant, I made a mistake in the translation as I'm (luckily) not English from origin , it mean Carbon with it! http://en.wikipedia.org/wiki/Carbon_(disambiguation) |
Best regards, |
|
Follow us on