1/8/2023 9:33 PM | |
Joined: 9/27/2006 Last visit: 9/13/2025 Posts: 12408 Rating:
|
Hello problemoops; Ivan has given you an excellent analysis of your communication setup, I wuld like to add a few important details that might come up in your projectAnd h You are using an Anybus X-Gateway Profibus master to Modbus RTU slave, correct? So, on the S7-300 side, you must configure the CP 342-5 as a Profibus-DP slave. The screenshot below shows how you would configure this on the nybus Nettool configuration software, The Anybus gateway actig as master, the CP 342-5 acting as slave. Look at the Notes on linking a CP 342-5 as a slave to a S7-300 system, and notice the requuirement for functions DP_Send and DP_Recv when you are working with a CP 342-5: https://support.industry.siemens.com/cs/ca/en/view/15007089 The link to the CP 342-5 gsd file, so that you can integrate it as a slave in the Anybus NETTool configurator is included in the link above: This document shows the use of DP_Send and DP_Recv in a CP 342-5 configured as DP-master. The requirements are the same if the CP 342-5 is configured as a slave. https://support.industry.siemens.com/cs/ca/en/view/18208090 Am=nd here is the link to all required documentation on the Anybus X-Gateway Profibus Master to Modbus slave. The manual on Profibus-DP master has been examined. You will have to configure the Modbus slave side based on the documentation you have on your Modbus aster system in your project. Th DGU must act as a Modbus master in this case. Hope this helps, |
Last edited by: dchartier at: 01/08/2023 21:37:48Last edited by: dchartier at: 01/08/2023 21:39:24 |
|
This contribution was helpful to
1 thankful Users |
1/9/2023 5:23 AM | |
Joined: 2/22/2022 Last visit: 1/9/2023 Posts: 7 Rating:
|
This is my really bad I miss to say thank you for advice. My head blows off there are lot of things to do, sorry. |
Follow us on