7/5/2013 10:56 AM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
BLKMOV in SCLSolution from Smiffy: [code]FUNCTION_BLOCK FB12 Best regards Hamid Hosseini |
This contribution was helpful to
3 thankful Users |
7/5/2013 1:51 PM | |
Posts: 55 Rating:
|
Dear hdhosseini, Thanks for the quickanswer. It worked well... Thank you so much. Regards, Prasad |
2/17/2014 7:47 PM | |
Posts: 340 Rating:
|
new question is splittet to Do you have this code but then for a s7-1200 plc (1214C). |
10/21/2014 4:02 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
|
11/5/2014 6:34 PM | |
Posts: 3 Rating:
|
The rest of code is copied from the previous posts. But when CPU executes the code, no data are copied. So I just wanna know if the definition of pointer is correct. I used the start of the DB (0. byte), because there is no way to make a mistake with addresses. I dont now now where is the problem.
AttachmentSCL Source.pdf (679 Downloads) |
1/23/2015 2:30 PM | |
Posts: 4 Rating:
|
The beauty of SCL is that offers you, like the saying says "1000 ways to skin a cat"
Attachmentcopy_data.zip (865 Downloads) |
Last edited by: uvcontrols at: 1/23/2015 2:42 PMLast edited by: uvcontrols at: 1/23/2015 2:39 PMLast edited by: uvcontrols at: 1/23/2015 2:37 PM |
|
This contribution was helpful to
2 thankful Users |
Follow us on