10/14/2014 1:31 PM | |
Joined: 11/21/2007 Last visit: 7/25/2025 Posts: 2326 Rating:
|
Hello KonradR This is what I can make out : - PLC Went to Stop in the First Program Cycle when switched from Stop->Run ) - At the time of Stopping PB96 was being executed at Relative Address 0068 Hex - No DB was Open - Fault Occurred - QVZ - Timeout ( Peripheral I/O Module ) Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
10/14/2014 9:20 PM | |
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating:
|
You need to look at the block in IL.Left are then available addresses. |
10/14/2014 9:33 PM | |
Posts: 97 Rating:
|
You need to look at the block in IL.Left are then available addresses. Gruß 190B I understandthat this adress corresponds to 0068 in STL Best Regards Konrad ![]() |
3/4/2015 9:37 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
|
Follow us on