1/8/2016 3:25 PM | |
Joined: 6/5/2014 Last visit: 7/21/2024 Posts: 109 Rating:
|
Many thanks |
4/9/2016 5:41 PM | |
Joined: 10/8/2015 Last visit: 3/1/2023 Posts: 59 Rating:
|
thanks ayman; urgent problem i want to use this example in my project which related to PM(maintenence). in my project there are a bout 30 motors .when i start each motor and get feed back this time must be calculated and when reach to my set point it must give alarm(it means time of meantenence).on the other hand operator should be check time or remaine day in wincc .can you help me how can i do it for 30 motors with only one fb1 and one datablock for all motors. when i executed program example (pegaia) i face on big problem in fb2 .so when i call fb2 ( fb2 call in fb3) i created two input seprate i0.0 and i 0.4 and two seperate output (slide1).but fb2 only run when two input areactive why? and time calulate together.this block must work when enable is (motor run) active seperatly and operator check time of each motor seperatly. best regards Attachmentslide1.pdf (576 Downloads) |
This contribution was helpful to
1 thankful Users |
4/30/2016 2:02 PM | |
Joined: 10/8/2015 Last visit: 3/1/2023 Posts: 59 Rating:
|
Dear Sir, DO your example has Limitation time (max 24 day).? can i use it for more than 24 days?. best regards |
7/1/2016 8:54 PM | |
Joined: 6/27/2013 Last visit: 5/9/2025 Posts: 29 Rating:
|
hello all can I build hour meter via wincc v7.3 time? my idea in wincc side |
Follow us on