10/24/2019 9:08 AM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35962 Rating:
|
I did tests. From this it can be seen that the data log is also written if the buffer is not yet filled with 512 bytes. Data Logs are attached. AttachmentData Logs.zip (388 Downloads) |
10/24/2019 10:26 AM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35962 Rating:
|
Here have news. AttachmentData Logs.zip (294 Downloads) |
10/24/2019 2:57 PM | |
Posts: 7 Rating:
|
Thanka all for replyes. 1. When I trying get DataLog via LSC I receive massage "No datalog found". 2. If I stop Logo and remove SD Card and read them in PC then I found zero length csv file (Program worked 1 week before read SD card) 3. Programm and screenshot of DataLog block properties is attached. AttachmentData Logs.zip (324 Downloads) |
10/24/2019 3:30 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35962 Rating:
|
Hello Nopolis, please be so Kind and upload you program as a ZIP file. Thanks. |
10/24/2019 6:25 PM | |
Posts: 7 Rating:
|
Program in attached zip file
AttachmentVer 9.zip (311 Downloads) |
This contribution was helpful to
1 thankful Users |
10/24/2019 7:19 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35962 Rating:
|
First transferred your uploaded program to my LOGO! 8.FS4. In attachement: AttachmentData Logs.zip (310 Downloads) |
10/24/2019 8:13 PM | |
Joined: 2/22/2008 Last visit: 4/25/2025 Posts: 2698 Rating:
|
Once again a destroyed program, which can be uploaded to the Logo and don't have all functions. |
10/24/2019 8:23 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35962 Rating:
|
I suggest the User Nopolis to start a Support Request so that Siemens will examined his source program. |
This contribution was helpful to
1 thankful Users |
Follow us on