4/20/2018 11:42 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2150)
|
Hello Labirex_Batyu, if would not like to use operatormessages, you could write entries direct in the AuditTrailDatabse by using the function "InsertAuditEntry". But this function does not check too, if the comment is not empty. That means you could create an own function "InsertAuditEntry", which checks, if the comment contains some characters. Regards Georg Berghof AttachmentInsertAuditEntry.txt (273 Downloads) |
PS: If this post did really help you, you may use the Rate-button |
|