11/4/2014 11:54 AM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Hello rockie86, Just to add some points to this discussion.The "attach symbols..." option in PLCSIM 5.X searches for a file with ".s7p" extension to distinguish it as a project.This extension is only created for classic STEP 7 projects and it can not recongnize structure of a TIA Project. This is why you can not find your TIA symbols to select in PLCSIM5.X.For me if it is really necessary, I export my symbols to an excel file (select all-->copy-->paste) and edit them in form of classic STEP 7 format (removing % from absolute addresses).As a work around, I make a project in STEP 7 with only an S7 program and then import the symbols there.In this way , you can import your important tags via PLCSIM 5.X.
About comments from our friend "huggy_d1", I guess he was talking about downloading a project related to S7-1500 in PLCSIM V1X.For S7-300/400 only blocks folder is transferred to PLC that doesn't contain any symbol file.This is as the same as PLCSIM V5.X. I hope this helps, Hamid Hosseini |
Last edited by: hdhosseini at: 11/4/2014 12:29 PMLast edited by: hdhosseini at: 11/4/2014 11:56 AM |
|
This contribution was helpful to
2 thankful Users |
11/4/2014 12:33 PM | |
Joined: 8/11/2011 Last visit: 5/17/2025 Posts: 51 Rating:
|
Thanks. This is what i wonder. But i dint understand why we are not able to attach symbols to PLCSIM in Tia portal? It is a need for all of us. Hope Siemens will solve this problem soon, Special thankshdhosseini...
|
Follow us on