10/28/2021 10:04 AM | |
Joined: 9/27/2016 Last visit: 12/30/2024 Posts: 6 Rating:
|
Hello Ever since installing PLCSIM Advanced V4.0 (had V3.0 before and older versions before that, no issues there) I'm getting a Windows Blue Screen every time I log on to my VPN (also when not using PLCSIM Advanced at all, and even without having TIA installed). Our IT department have tracked the issue to PLCSIM Advanced related files (also - this started happening right after installing it with no other special changes), but have not been able to fix the issue. We've even tried formatting the entire machine and installing it anew from scratch, but after installing PLCSIM Advanced 4.0 the issue again persists. We use Pulse Secure VPN. You can imagine working from home often requires a lot of both these tools (PLCSIM Advanced and VPN...) so this issue is really hurting me currently. Any ideas are welcome ! |
10/28/2021 10:08 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
check that the SIMATIC insustrial ethernet ISO Protocoll is not activated on the VPN Adapter |
10/28/2021 11:00 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
can you provide the crashdump/minidump which BSOD exactly happen? |
10/28/2021 12:15 PM | |
Joined: 9/27/2016 Last visit: 12/30/2024 Posts: 6 Rating:
|
Sure, here's the mini-dump (need to rename back to .dmp). The full dump is 66GB... The Stop code is KMODE EXCEPTION NOT HANDLED. What failed: ndis.sys. Attachment102821-19359-01.pdf (600 Downloads) |
Last edited by: GalSnir at: 10/28/2021 14:14:26 |
|
1/5/2023 5:30 PM | |
Joined: 6/13/2019 Last visit: 4/29/2024 Posts: 3 Rating:
|
GOD!! It is working! Thank you VERY VERY MUCH! |
Last edited by: AutoGen_3650279 at: 01/05/2023 17:58:05 |
|