5/19/2017 8:21 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, there is no adress for run,fwd,rev,speed or speed reference in the G120! The G120 dosn't work in this way over profinet! With Profinet the communication between PLC and Drive is implemented with the PROFIDrive Standard. With this you have defined Telegrams with Control and status words and Speed values in the Telegram. To control the drive you use the technology object and the Motion Control Commands and with this the PLC create the telegraminformation and sen it to the drive. The received data are interpreted and used in the drive. You can also use the Drivelib function blocks to control the drive: https://support.industry.siemens.com/cs/ww/en/view/109475044 Regards Christoph P.S. please stop quoting ! only click on answer! |
Last edited by: ChristophD at: 5/19/2017 8:25:57 AM |
|
Follow us on