7/25/2019 11:34 AM | |
Joined: 6/1/2018 Last visit: 12/11/2023 Posts: 18 Rating: (0) |
Hi I'm not very expert at all Siemens world. And I have a question for a very expert of development program in TIA V14. I have in my hardware configuration a device with more access a single byte . I'm sorry for my english, it is very bad. For help my I send an attach with my hardware configuration. I would to make a FB with a singl paramiter in input to access at all byte of this device. I don't know if this is possible. At moment I need write more part of progrma to access at all byte of periphery. But if is possible to have a paramiter in input of FB and also to address the read of periphery with this paramiter I can make a loop to read all byte with a simple part of program. I use this tecnology for read and write a DataBlock, for exemple when I have a tracking. But this is possible if I point to hardware addresses?? I send also a list of system variable. In this list are present all byte of my device at format "Hw_ SubModule", and I noticed that the values of these variables are consecutive. That is ideal situation for read all with a loop. Tank you for all
AttachmentSystem Configuration.pdf (76 Downloads) |