9/15/2014 3:38 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello Shreyas No, we finally used S7redconnect for this project as we did not want to experiment. However I strongly suspect that the Redundancy script for connecting Soft Redundancy systems ( SWR ) to winCC should also work with S7-400H. ( Although SIEMENS will probably never confirm this officially ) More Details in this Thread : Redundancy PLC System communication with WinCC Pl check out thus post byTagolover :
Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
10/23/2015 7:40 PM | |
Joined: 9/2/2012 Last visit: 4/18/2024 Posts: 711 Rating: (30) |
Dear Navnag, you could able to try anything further on this concept ? currently am also looking for the similiar solution, but no H-system available with me to try. Anybody have resources to try below setup with create redundant connection option in wincc side? H-Wincc Communication over profibus |
|
|
8/24/2017 8:52 AM | |
Joined: 8/21/2014 Last visit: 5/22/2024 Posts: 959 Rating: (13) |
New question published by s_vb is split to a separate thread with the subject Want to communicate WINCC 7.0SP1 with my laptop without using CP card.. Best regards |
Last edited by: Jen_Moderator at: 8/25/2017 9:43:36 AMInserted right thread-headline. My Forum is the place to personalize your profile, |
|
Follow us on