11/15/2013 3:30 PM | |
Posts: 1299 Rating:
|
Hello, you can use a plc tag to reset the alarms K!ke |
11/19/2013 8:27 AM | |
Joined: 10/8/2008 Last visit: 7/2/2025 Posts: 43 Rating:
|
Hi all in the jpg file you can see the button. How is it possible to get this (bool) in the PLC logic. Jan. |
11/19/2013 2:24 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello JanLan, I've found the following link: how can you determine the bit number in WinCC for the "Trigger address", the "Acknowledgement PLC" bit and the "Acknowledgement HMI" bit for creating bit messages? It's about WinCC flexible, but perhaps you can use it in WinCC. Best regards, Wizard |
11/19/2013 3:38 PM | |
Joined: 10/8/2008 Last visit: 7/2/2025 Posts: 43 Rating:
|
Hi Wizard, As you can see in the discrete alarm window I do not have alarms there I used the new block in the S7-1511 Program alarm and Get AlarmState. Alarms are the automaticaly generated in the HMI. in de controller alarm window. The construction you pointed to I know how that works Thanks for the reply Jan AttachmentAlarm.zip (543 Downloads) |
11/20/2013 4:14 PM | |
Posts: 1299 Rating:
|
Hello, you can also configure your own button to reset the alarms and hide the one which is in the alarm view. K!ke |