6/25/2013 1:58 PM | |
Posts: 319 Rating:
|
Dear CesarL, Have you selected WinCC OPC Server option while installing WinCC Software ? Check the attachment , it will give you a clear picture. With regards, nand gate.
AttachmentWinCC.zip (691 Downloads) |
1/9/2015 3:31 PM | |
Joined: 2/6/2009 Last visit: 6/10/2024 Posts: 46 Rating:
|
Hello, Today, I had the same issue with WinCC V70 SP3 and Simatic Net V8.1 SP1 installed on PC running Windows Server 2008 R2 Standard SP1 x64 edition. In Station Configurator of Simatic Net was no WinCC application offered in add component menu, even these software's are correctly installed. In compatibility lists, all software packages are represented as compatible. I tried to import station with xdb file, but got message "The component is not installed". Several reinstallations with different order were generating the same problem, no matter what. After applying a service request I got the solution that fixes this issue. See attached files. Hope this will help to others. Best regards, VladD AttachmentWorkaround_WinCC-Application_EN.pdf (1382 Downloads) |
This contribution was helpful to
10 thankful Users |
1/9/2015 3:32 PM | |
Joined: 2/6/2009 Last visit: 6/10/2024 Posts: 46 Rating:
|
And second file. P.S. I cannot attach 2 files in one post? Why? Best regards, VladD
AttachmentFix.zip (1073 Downloads) |
Last edited by: VladD at: 1/9/2015 3:32 PM |
|
This contribution was helpful to
10 thankful Users |
2/11/2015 12:30 PM | |
Joined: 9/29/2005 Last visit: 6/19/2024 Posts: 5 Rating:
|
Works also on Win7 SP1 x64 Simatic NET V8.1.2 |
5/31/2015 2:24 PM | |
Joined: 4/14/2015 Last visit: 6/19/2024 Posts: 8 Rating:
|
thanks my problem is solved |
Last edited by: vagish1111 at: 5/31/2015 2:24:27 PM |
|
7/1/2015 3:49 PM | |
Joined: 9/19/2013 Last visit: 7/2/2024 Posts: 21 Rating:
|
Thank you Sir. |
4/15/2016 12:15 PM |
|
Joined: 7/13/2009 Last visit: 6/3/2024 Posts: 137 Rating:
|
|
Thanks and Regards |
|
Follow us on