12/1/2019 5:46 AM | |
Joined: 11/20/2017 Last visit: 5/23/2024 Posts: 2 Rating: (0) |
Hi I have the same problem Adonis were having. I'm using Starter Es V14Sp1 and also suddenly the profibus dp communication stops. I have a MCC with 68 motors three 3rw44 soft starters for 132 Kw and the others with simocode pro c.I don't have problems with simocodes but i do have problems with the 3rw44. 1 Suddenly communication stops 2 When I start the soft starter an error shows in the display.It says supply voltage is 110% but it does starts first. The soft starters are being used for mills. I would be glad if you could send or give me an answer. My mail is [snip]. If you need some other datas to be clear, tell me. Thanks I'm hoping SIEMENS has been always my first choice ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/02/2019 06:15:23New subject after splitting. Removed E-Mail address. |
|