3/21/2018 12:19 PM | |
Posts: 13 Rating:
|
Add: i want to use telegram 111 and with PLC control only target position, velocity and override (and read actual values). Thats enough in soooo many app... |
3/21/2018 12:25 PM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
then use GSD/GSDML and the problem is solved, so what? |
3/21/2018 12:38 PM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hi, you can also create the CU320-2 in TIA, but don't connect to the S7-1200. The configuration of the drive can then be done in TIA. you can also open a support request and ask why only S7-1500 is supported , but i think you will not get a really helpfull answer. Regards Christoph |
Follow us on