1/10/2015 8:13 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi, A new feature that WinCC V13 SP1 brings is the pop-up images that accentuate their functionality by their animated appearance. The object is available in Runtime Advanced, the Comfort Panels and in our new 2nd generation Mobile Panels. Note: as from TIA V14, it is possible to open the pop up with different sizes by "ShowPopupScreenSizable" function AttachmentPopUP.zip (4431 Downloads) |
Last edited by: Denilson Pegaia at: 2/27/2017 12:47:59 PMDenilson Pegaia |
|
This contribution was helpful to
8 thankful Users |
1/11/2015 1:08 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
... an application example is to use it as "command confirmation window". Here there is an example of that. AttachmentPopUP2.zip (3011 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
1/11/2015 1:10 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
... and, as "multi command confirmation window", like here: AttachmentPopUP3.zip (2774 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
4 thankful Users |
1/16/2015 10:22 AM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi, this feature is just available to Comfort HMI + WinCC V13 SP1. You can download the SP1 at STEP7 http://support.automation.siemens.com/WW/view/en/105825934 WinCC http://support.automation.siemens.com/WW/view/en/106567433Startdrive http://support.automation.siemens.com/WW/view/en/68034568 |
Last edited by: Denilson Pegaia at: 12/14/2015 7:19:03 PMDenilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
1/19/2015 10:39 AM | |
Posts: 116 Rating:
|
I'd like to try this pop up feature. But I can't open project (see in attached photo). I also has my list of installed SW which export out from TIA portal. please, let me know what I really need to installed to be ableopen this pop up project. I'm a bit confuse with different of WinCC and TIA portal. Thanks. AttachmentForum.zip (1056 Downloads) |
1/20/2015 7:33 AM | |
Posts: 1299 Rating:
|
Hello, you need Service pack 1 to use this feature. see the links in Pegaia's last answer. K!ke |
This contribution was helpful to
2 thankful Users |
1/23/2015 2:59 PM | |
Posts: 7 Rating:
|
I trie to innstal Comfort, but i get attached error. What can i do? |
2/6/2015 10:45 AM | |
Posts: 16 Rating:
|
Hi, Can you put some pictures about project tree and result on the HMI to have an idea, for user without V13 SP1 Thanks
|
3/26/2015 2:22 PM | |
Posts: 1299 Rating:
|
Hello, you can change the size in the properties of the pop up window. K!ke |
7/2/2015 12:29 PM | |
Joined: 11/6/2014 Last visit: 9/12/2025 Posts: 1 Rating:
|
where? I do not see the size change in the properties of the pop -up windows. Can you put any image capture ? Thanks! |
7/7/2015 7:00 AM | |
Posts: 1299 Rating:
|
See attached picture K!ke |
Follow us on