9/27/2017 6:31 PM | |
Joined: 2/10/2015 Last visit: 5/16/2024 Posts: 286 Rating:
|
thank you very much Mr. ALEX MOL, I will try but the worry is that I'm new to the company and when I look at the SCADA, I do not see where I need to increment #speed and also when I ask the machinist he tells me he does not know how to increase it. I want to ask if I can create a variable table to force #speed to 40.50 etc to see the state that M22.1 will take. the DB10.DBW96 is used twice in the program. Here is the ZIP file of the machine program. it is in the project (EXTRUDER) that FC187 is found and it is in FC23 that it is called. it is in the project (LINE) that is the automatic operation of the machine: FC109 network10 and when I select the automatic mode it is the contact DB101.DBX4.1 which does not close so that the coil M159.7 is activated to be able to start the machine, thank you and I am always online. is that you can show me as a screenshot how I have to put ("//") to turn off network 50 to see what's going on in network 51 and also i want to know if it's a program that is written in LADDER or in LIST in TIA PORTAL or SIMATIC MANAGER and a call of the same block is made several times, how we do to see the values of the different networks where the block is called Attachment40084c_P.zip (139 Downloads) |
9/28/2017 7:31 PM | |
Joined: 2/10/2015 Last visit: 5/16/2024 Posts: 286 Rating:
|
for the SCADA of which I spoke, it is a computer that is connected to the PLC for the control of the machine |
Follow us on