5/26/2015 12:45 PM | |
Posts: 76 Rating:
|
Hello, I have a problem with loading the WinCC V13 project via Pack&GO file. I did a downgrade of the firmware as OP requested. But the loading was unsucessful. I got a message that I don't have a license (WCRT031300). Can someone tell me what is this license for? For more information see the picture below (Pic1). Then I went into Transfer mode if this would help but it wasn't better. I got a message saying: "S7DOS component is missing" (look at the picture below Pic2). Does anyone know what can be the problem. Thanks for all your help. Best regards Lesko AttachmentScreenshots.zip (1475 Downloads) |
Last edited by: lesko at: 5/26/2015 12:47:17 PMLast edited by: lesko at: 5/26/2015 12:47:56 PMLast edited by: Min_Moderator at: 5/27/2015 1:33:28 PMMove pictures to attachment |
|
5/26/2015 2:14 PM | |
Joined: 8/3/2009 Last visit: 9/1/2025 Posts: 16284 Rating:
|
Hello lesko I Think you have to install the SIMATIC Prosave too. The S7Dos Driver ist also installed with Prosave You can use the download here: https://support.industry.siemens.com/cs/ww/en/view/10347815 Good Luck Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
5/9/2016 3:37 PM | |
Posts: 20 Rating:
|
Just checked, got all requirements. |
Follow us on