2/8/2022 10:13 AM | |
Joined: 11/2/2021 Last visit: 2/18/2022 Posts: 10 Rating:
|
Hello there, I also had the same problem. Tried to set a static IP but it was totally overlooked by the system. When I wanted to look up the configuration, I noticed that the directory '/etc/netplan' doesn't even exist after the system has been installed on the IOT2050. The IP is automaticly DHCP in both ports, even though it was said that P2 would be static and P1 would be dynamic. How do I enforce a specific IP-Address at startup? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/08/2022 13:19:16New subject after splitting |
|
Follow us on