5/11/2022 8:42 PM | |
Joined: 3/14/2008 Last visit: 9/17/2025 Posts: 2217 Rating:
|
Hi, Thank you for your tip. The workaround is listed in the compendium part C though. Whenever problems arise, remove the EM role assignment, update and reconnect to establish the block contacts again. See chapter 10.3.8 in the manual: Compendium part C As a general tip: Please follow the manual precisely! Procedures must be followed in an exact way, otherwise problems could arise. For example, when an EMT is used a lower level EM in an EPHT, and the EMT is changed (new characteristics for example), please note that there is a specific update procedure-> Update SFC block type of the EMT, update block contacts at the EPHT, update SFC block type of the EPHT etc.
|
Last edited by: Oreca at: 05/12/2022 10:33:01Insert link to compendium manual and reference to chapter If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
Follow us on