5/24/2022 8:52 PM | |
Joined: 8/29/2013 Last visit: 11/19/2022 Posts: 2 Rating:
|
Hello Sinumerik 840 D Power line Dear Expert Team, I need a help at this following subject- We have some Machines where the S7-Manager and the PLC Programm is installedat PCU 50 .when i want to compare the project (offline PLC Programm) wiht the PLC Programm at NCU comes a message that was impossible to conect.. From Set PGPC Interface i send here was programmed. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/25/2022 08:48:45New subject after splitting |
|
5/25/2022 6:42 PM | |
Joined: 10/17/2007 Last visit: 9/15/2025 Posts: 4452 Rating:
|
1st of all why you want to access PLC program. if you are end user , Siemens not suggest to do so. If you are service/maintenance person, I suggest you use stand-alone PG/PC (SIMATIC Manger installed) to all you need. --I am sure everything should be working smoothly For SMATIC Manage integrated inside PCU 50, Siemens already remind--that is for maintenance person basic check and troubleshooting. I myself really use this function in the service (only 1% other 99% I use PC) . I don't remember what's wrong with your case --from you picture, we can see PCU connecting to OPI (1.5M baudrate) . do you input password-- SUNRISE. you want to compare PLC program. but do you make this PCU50 (SIMATIC Manger ) online, I mean you can read Program? also do you know the story of this machine? such as machine possible being upgrade to higher SW version and SIMATIC Manager is too old?
|
Last edited by: nulizhang at: 05/25/2022 18:43:04If you like my comments please |
|
Follow us on