5/23/2022 3:49 PM | |
Joined: 5/20/2022 Last visit: 5/23/2022 Posts: 1 Rating:
|
I have tried the "840d PL NC___PLC_Data_Clear & restore procedure.pdf" procedure multiple times with no results. NC & PLC clear procedure works up to line #9 but on line #10 PS LED does not show blinking (Stays solid red). Then when executing Line #11 +5V and PR go green and PS goes out. I don’t think NC & PLC are clearing from the control or something else is wrong. I had this problem back in 2015 and the procedure worked fine. Then on "NC Data reload" everything seems to work up to line #23 and Line #24 “communication to NC re-established” comes on for just a brief second then goes right back to “Communication to NC failed” I’m at a loss please help. Gordon ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/24/2022 06:14:16New subject after splitting |
|
Follow us on