10/31/2022 7:55 PM | |
Joined: 10/4/2019 Last visit: 3/28/2025 Posts: 120 Rating:
|
|
11/3/2022 5:54 PM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35946 Rating:
|
Import of a technical question via PM from the user adamlahadi. ln ths s7-1200 firmware V4.2 manual page 89 it's mentiond that in the startup process the CPU copies the state of the physical inputs to the I memory,in page 90 under startup processing it said the opposite of that so in the startup ob100 i put (NO i0.0) to set Q0.0 ,so as a resault and before the CPU goes to run mode the Q0.0=1, so we can say that what was mentioned in page 89 (D) was true not page 90 which tells you that (for my case ) that i need to perform an immediat addressing in order to set the Q0.0 (NO I0.0:p) to set Q0.0 i found a contradiction between the two pages 89/90 or it's a miss understanding from me can you help with that kind regards |
Follow us on