1/6/2023 7:11 PM | |
Joined: 1/21/2013 Last visit: 9/11/2025 Posts: 4102 Rating:
|
Hi bejb,
if you work with a S7-1200 PLC, you can use either the internal load memory or a SIMATIC S7 memory card to store the program data. This means that you can replace the built-in memory with a memory card, but you cannot combine the two memories. So to use more than the built-in 4 MByte, you need a memory card that is bigger than this 4 MByte. For more details take a look at "How can you use the memory card for the S7-1200 CPU?". Kind regards |
This contribution was helpful to
2 thankful Users |
Follow us on