9/23/2022 6:15 AM | |
Joined: 7/25/2016 Last visit: 9/23/2022 Posts: 1 Rating:
|
I want an Expansion module for my S7-1200 COU , I need min 250 input and 250 Output with 10 analogue input and output , Please help to give me a part number ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/23/2022 09:53:34New subject after splitting |
|
9/23/2022 1:50 PM | |
Joined: 7/7/2010 Last visit: 9/17/2025 Posts: 16110 Rating:
|
Try out the TIA Selection Tool on this support site. You can specify as many IO modules as the selected s7-1200 can support. To meet the I/O requirements, you can quickly determine how many additional S7-1200's (configured as I-Devices), or other remote I/O system, and I/O modules are required to meet your project needs. With that many I/O points, in the interest of reducing the number of wires and cables "home run" back to the main PLC enclosure, remote I/O systems are definitely a big wiring and cable tray time, space and cost savings option.
|
science guy |
|
3/1/2023 7:39 AM | ||||||||||||||||
Joined: 9/9/2017 Last visit: 9/10/2025 Posts: 7 Rating:
|
hi s71200 plc can be add max 7 expansion
REG G.Venkat |
|||||||||||||||
Follow us on