3/7/2023 12:13 PM | |
Joined: 1/24/2021 Last visit: 8/29/2025 Posts: 118 Rating:
|
Br |
Please feel free to rate my contribution if it was helpfull :) |
|
This contribution was helpful to
1 thankful Users |
3/8/2023 11:02 AM | |
Joined: 1/21/2013 Last visit: 9/8/2025 Posts: 4093 Rating:
|
Hi KevinNfoDrives, Reading manuals always has something to do with experience. And so is the author of the manuals. There is no general definition of what information is where. At best, there are company guidelines to ensure that manuals are structured in a similar way within a company. Everyone has their own preferences and may find one manufacturer's manuals better or worse than another. In this case, at least the information you want will be in the manual. The picture posted by gvatte shows the SM 1223, but the wiring of the internal inputs is the same. However, M is not always connected to 1M. The important thing is that 1M is used to close a circuit. By the way, BR is used as an abbreviation for Best Regards. So, best regards |
Follow us on