11/22/2020 11:46 AM | |
Posts: 1 Rating:
|
dear expert I need support , when I make migration from op77b to Kp 400 comfort ,the arrows keys that navigate between pages become not activate ,although , when I check a program after migration it has event in program ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/23/2020 07:55:05New subject after splitting |
|
11/23/2020 8:01 PM | |
Joined: 2/6/2015 Last visit: 8/12/2025 Posts: 80 Rating:
|
Hi ibrahim gawad, When you do a migration the assignment of an old function key could be assigned different numbers on KP 400 Comfort. Revise this assignment. I would recommend download the Comfort Panels Migration Guide: https://support.industry.siemens.com/cs/us/en/view/49752044/44564143243 Best Regards, CGA81 |
If this Information really helps, you could use the Rate function |
|
5/19/2023 12:02 PM | |
Joined: 1/19/2021 Last visit: 5/19/2023 Posts: 1 Rating:
|
Hey Guys, So I am posting on this thread as I wanted to write the same title. What would you suggest as best practice to read the data from the OP77B or MMC card so I can migrate, update and transfer it to the KP400. |
5/26/2023 7:48 AM | |
Joined: 8/3/2009 Last visit: 9/16/2025 Posts: 16436 Rating:
|
Hello USB Adapter and USB Adapter A2 are only released for transfer to:
But not to OP77B -> Manual you would find here: https://support.industry.siemens.com/cs/ww/en/view/21084916 Also you cannot do a Backup and change something in it. here you would need a working project for WinCC flexible or TIA Portal. If you do not have the project and want to migrate, this could be an option for you: https://support.industry.siemens.com/cs/de/en/view/109765132 Bye Murof Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on