6/8/2023 10:56 AM | |
Joined: 6/3/2023 Last visit: 9/13/2025 Posts: 2 Rating:
|
Hello could you please tell me the IP address , subnet mask & Default Gateway used here are from the same series of router or what, apart from these settings do i need to change anything in router side , HMI & in TIA Project ? Because i am using TP1500 HMI , X1 Port is in connection with PLC with same series of IP address, x3 port ip addresss in same series of router, but when i try to access browser in hmi it gives me an DNS error page.. so please anyone help me it working me for only in simulation not when i connect it to router through LAN. can anybody tell in brief complete steps to follow one after other.. Thanks in advance
------------------------------------------------------------------------------------------ |
Last edited by: amar_bira_dar at: 06/08/2023 11:01:03Last edited by: Jen_Moderator at: 06/09/2023 09:29:33New subject after splitting |
|
Follow us on