9/11/2023 1:13 PM | |
Joined: 6/29/2023 Last visit: 1/13/2025 Posts: 21 Rating:
|
Hello, I am working with a Project in PCS7 and a Panel Confort in Tia Portal. In order to import the project alarms, I followed the documentation 50708061_application_pcs7_panel_integration. The alarms in the step7 project are working correctly however, when I want to import them in TIA Portal, they don´t trigger when they have to. Despite they don´t function in runtime, in TIA portal the alarms appear rightly. What can I do to activate them? Thanks for advance. |
Last edited by: U_0579f805-6793-42c7-be9c-feec42a323a8 at: 09/11/2023 13:17:26Last edited by: Jen_Moderator at: 09/12/2023 08:03:59Link embedded. |
|
9/14/2023 7:08 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Project PCS7 Alarms in TIA portal is published within the conference SIMATIC WinCC (TIA Portal). Jen_Moderator |
Follow us on