9/27/2023 4:55 AM | |
Joined: 8/11/2021 Last visit: 9/8/2025 Posts: 10 Rating:
|
Hello, did it worked? Actually i want to ask if it was just ''plug & play'' or the commissionig was required? I have the the same old card and i think it is broken. The new card is coming. I have tried in the software offline to switch it but it is not working so i need to delete the old card, inserate the new one and configure it. Siemens is saying that the card is the succesor so i have expected to switch it without further commissioning. I do not have experience with this card and i would like to know what to expect so i can be ready when the card is there. The software is Step7 v5.6. Thanks in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/27/2023 10:03:08New subject after splitting |
|
Follow us on