10/13/2023 4:36 AM | |
Joined: 3/30/2020 Last visit: 9/5/2025 Posts: 5427 Rating:
|
Yes, it is possible to have the hardware and software load from the card to the PLC. Even the IP address can be set in this way. The card must be a special Siemens Memory Card which makes it expensive. Not all regions carry the card in stock, so you need to make enquiries. Get the S7-1200 System Manual. The manual contains the part numbers for the memory cards. The procedures to follow to prepare the card is also documented. There are several ways of preparation. it is possible to have the card need to stay inside the PLC or the card becomes blank after doing the transfer. You must make a study of the procedures. Unfortunate SiePortal is not working properly at this moment, so I cannot give you the link address for the manual. You will have to search for it yourself. Good luck. |
Last edited by: qwazee at: 10/13/2023 12:35:41Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
10/13/2023 4:59 AM | |
Joined: 3/28/2015 Last visit: 8/15/2025 Posts: 725 Rating:
|
Hello, Perhaps the following topic might help: SIMATIC Automation Tool - the commissioning and service operation tool for SIMATIC modules |
Eng.Mohamed Ibrahim |
|
Follow us on