10/17/2023 1:53 PM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hi Ian, can you give a bit more information please? Are you referring to THIS document? Do you have a part number of the drive? Ideally a parameter list ... if possible Number of motors in parallel? Total power rating of motors (Maybe a photo of the motor plate and wiring) Has the Imax been set to the sum of all motor currents? Wiring configuration inside the motor terminal box? Are the motors identical - very important Length of motor cables - approx should be fine Are there any output components in the motor cable line i.e. output choke, sine wave filter etc? Actual fault code, and any warnings spotted before trip occurs. Think that's it for now Regards, Graeme |
Follow us on