11/29/2023 5:57 PM | |
Posts: 2 Rating:
|
Hi Everyone, I currently have a Siemens controller CPU 1214C, DC/DC/DC 6ES7214-1AG40-0XB0 with the article number 6ES7214-1AG40-0XB0. I am experiencing difficulty connecting a safety light, specifically the Dinfu 30W LED Forklift Light Safety Light Warning Truck Work Spot Light DC 12-80V (Red) from Amazon.co.uk, to the output of the controller. The issue arises because the switching capacity of the controller's output is 24V, 0.5A, and a maximum of 5W, while the safety light requires 30W of power to operate. Additionally, its working voltage is around 12-80V, and if it receives an output of 24V, the current should be a minimum of more than 1.25A. The problem is that the controller is unable to provide enough current supply to the load, which is the safety light. I am also unclear whether the supplied power from the controller's output is 5W in total for all outputs or if it applies individually to each output of the controller. Safety Light Link: Dinfu 30W LED Forklift Light Safety Light Warning Truck Work Spot Light DC 12-80V (Red) : Amazon.co.uk: Automotive Siemens Controller Datasheet: Product Details - Industry Mall - Siemens Great Britain Any explanations, suggestions or solutions to resolve this issue would be greatly appreciated. Thanks in advance! |
Last edited by: AutoGen_1293723 at: 11/30/2023 15:45:39 |
|
Follow us on