1/3/2024 8:36 PM | |
Joined: 8/14/2021 Last visit: 10/23/2024 Posts: 17 Rating:
|
Hello everyone, I don't know if the problem I have is related to this thread, if so I apologize in advance, I have an S7-1215, with a user page, I have opened port 80 on the router, from within I can access the network without problems, but I cannot access it from outside. Testing the ports from outside tells me that port 80 is not open. In the web server configuration, the default gateway appears at 0.0.0.0. I don't know if this is the one. problem, but I don't know how to change it, can you help me? I attach screenshots. thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/04/2024 09:38:48New subject after splitting |
|
1/5/2024 3:37 PM | |
Joined: 8/12/2021 Last visit: 8/20/2025 Posts: 351 Rating:
|
Are you using a VPN tunnel? Try opening the alternative port for HTTP 8080 |
If this Information really helps, you could use the Rate function |
|
1/14/2024 8:15 PM | |
Joined: 8/14/2021 Last visit: 10/23/2024 Posts: 17 Rating:
|
Ya he encontrado como poder introducir la ip del router y habilitar lo. Muchas gracias. |
Follow us on