2/16/2024 1:05 PM | |
Joined: 10/6/2010 Last visit: 11/18/2024 Posts: 14 Rating:
|
Good Morning I have two couples of redundant CPU's, 410E e 412 5H connected using two ethernet cables On CPU 410-E i am using the ports X8 on the 412-5H I' am using two CP-443-1. In S7 configure Network. I Have create 2 connections "S7 fault tolerant" between the Cpu's. (Image 0) Connections are named 1 and 2. I create inside the connections the link between the port X8 of the cpus'410-E nand the CP-443-1 (Image 1 and 2) In the S7 program i have two SFB , SFB12 and 13 and i have to exchange 200 bytes between the cpu's . Connection 1 for send data from 410-E to 412-5H and viceversa for the connection number 2. Both programs have B-SEND and B-RCV inside, a B-SEND and B.RCV for connection 1 and the same for connection 2. B-SEND is called with the connection number 1 when the connection is declared active (Images 3 e 4) In both cpu's the blocks ends with the error and status at value 1. (Image 4) And the data are not exchanged, the error (image 5) is not clear for me, and online i haven't found any info on it. Someone have any idea regarding this issue??? Thanks in advance Attachmentimages.zip (498 Downloads) |
2/21/2024 11:50 AM | |
Joined: 8/3/2009 Last visit: 9/9/2025 Posts: 16368 Rating:
|
Hello Guderian Perhaps in this FAQ there are a few useful information: https://support.industry.siemens.com/cs/ww/en/view/43033406 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on