2/27/2024 9:25 AM | |
Joined: 8/3/2009 Last visit: 9/15/2025 Posts: 16409 Rating:
|
Hello Kcy1019 there are only a few native communication drivers available for the Basic Panels 2nd Gen: for Profibus I know only the Siemens Channel Drivers. I think there is no communication driver for beckhof PLCs available. There are also no GSD Files for Basic Panels 2nd Generation available because the Communication is not like a PN/IO or DP/IO like a ET200. There is a HMI communication used which you do not need to use inside the hardware config of a PLC. So you have to look if you could use one of the existing communication drivers but I never used Beckhof with this Panels If you would need a Comfort Panel or Unified Comfort Panel then you could also use OPC UA (ethernet): https://support.industry.siemens.com/cs/de/en/view/109772341 But Basic Panels do not support OPC UA (and this one with DP also not Ethernet...) Bye Murof |
Last edited by: Murof at: 02/27/2024 09:27:59If this Information really helps, you could use the Rate function |
|
Follow us on