(0)| 8/12/2024 9:36 AM | |
|
Joined: 8/3/2009 Last visit: 1/19/2026 Posts: 16644 Rating:
|
Hello nnnayeem There are some HMI solutions that have a clould connector componet to get connected via MQTT for example WinCC V7/8 (LINK) WinCC Comfort/Mobile Panels or Basic panels do not have connectivity via MQTT implemented Also for Unified Panels there is no native driver implemented but here I heard of MQTT Edge apps. Almost all HMI devices (expect Basic Panels) an use OPC UA Server/Client connectivity Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on