10/8/2024 9:33 AM | |
Joined: 7/19/2022 Last visit: 9/16/2025 Posts: 436 Rating:
|
Hello AutoGen_3233562, Yes, you can work with the S7-400 and the HMI panel in TIA Portal or you can continue working with the S7-400 in STEP 7 Simatic Manager and the HMI panel in TIA Portal. Here is an application example of how to implement it: Combined configuration with WinCC (TIA Portal) and STEP 7 V5.x or Combined configuration with WinCC (TIA Portal) and STEP 7 (TIA Portel) in separate projects (Video) |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
2 thankful Users |
10/11/2024 12:11 PM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16447 Rating:
|
Hello Often you can also migrate old WinCC flexible Panels to TIA Portal. you wuold go this way if you only want to replay with new HW but keep the HMI Project https://support.industry.siemens.com/cs/de/en/view/76878921 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on