7/3/2023 9:43 AM | |
Joined: 1/21/2013 Last visit: 9/18/2025 Posts: 4111 Rating:
|
Hi Simon, First of all, you did everything right. I assume that you are not yet using the library with a large number of users, so you are simultaneously playing the roles of "Developer", "Integrator", and "User" as described in the "Guideline on Library Handling in TIA Portal". There are several reasons for using the corporate library. First, you may not want to have all versions ever released within that library. It should only contain the tested and released version. Another important reason, which you will only notice when more users are working with the library, is that a library can only be shared by multiple users if no one opens the library with write access. So if other users are already working with your library on a shared drive, you cannot make the library writable to make your changes. However, it can always be difficult to share a new version of the corporate library because you cannot replace the existing one with a new one until all users have closed the library. You can change the corporate settings so that a different library fill is used the next time the user starts TIA Portal. You can try to run a script that replaces the library during the night, when it is likely that all users have shut down their computers, or you can use a local copy on the user's computer that is replaced during the login process. Starting with TIA Project-Server V1.1 - which ships with TIA Portal V18 - this process becomes easier because the project servers also support libraries. Kind regards |
7/3/2023 9:57 AM | |
Joined: 3/25/2015 Last visit: 8/5/2025 Posts: 124 Rating:
|
Hi, yes I'm now the User/Developer/Integrator of this library, so it's just a testing environment. Our company didn't rely much on library feature in the past, but now we're dealing with a series of projects that require same type of FBs and FCs. I'm trying to standardize some common elements across all the projects. I think the solution to replace the library during the night can be the best. The only problem is how to notify the users about the new version released on the server, because some users are working from VPN remote site. The best would have been a "New version of the block FBxxx is present in global library Libxx. Would you like to upgrade the current project?" type of alert to notify the users about new versions. I've followed this guide https://support.industry.siemens.com/cs/de/en/view/109739199 and this article https://support.industry.siemens.com/cs/mdm/109773506?c=124509337867&lc=en-IT But I don't have access to every user PC to change the XML configuration. I would like to do that automatically by notifying the users. I think this lack of functionality is the only flaw in the library ecosystem of tia portal
|
Last edited by: Jen_Moderator at: 07/04/2023 06:02:20Link optimized. Kind regards |
|
Follow us on