12/4/2023 10:04 AM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi As from TIA V19, it is possible to configure a S7-1500 CPU (FW 3.1) to save security events internally to be read by a Syslog server (e.g. SINEC INS). Syslog is a standard protocol for forwarding log messages over IP networks. It is very common in the IT (Cibersec) world. A syslog server normally is a security / network manager software that collects the logs from the network devices. TIPs:
Sample project (archived from TIA Portal as .zap19 and after that compacted in .zip format to be uploaded here) including also print from Hercules getting syslog events. AttachmentSyslog.zip (549 Downloads) |
Last edited by: Jen_Moderator at: 12/05/2023 07:04:26Text formatting optimized. Denilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
12/13/2024 4:55 AM | |
Joined: 12/27/2021 Last visit: 9/17/2025 Posts: 3 Rating:
|
Can we route syslog messages via CP card of S7-1500 or ET 200SP CPU? |
Follow us on