9/21/2023 2:24 PM | |
Joined: 6/26/2023 Last visit: 9/2/2025 Posts: 25 Rating:
|
Hi Expert, I can ping both from my Laptop. AttachmentPLC_HMI.pdf (769 Downloads) |
9/21/2023 2:48 PM | |
Joined: 5/6/2022 Last visit: 9/15/2025 Posts: 589 Rating:
|
Hi AutoGen_1107196, Firstly, I would like to ask you if both PLC and HMI are simulated, does the communication between them work? I also leave you below some FAQs that can be very helpful in solving these problems: -> Connection configuration: "In WinCC (TIA Portal), how do you configure a connection between WinCC Runtime Advanced or HMI Panel and an S7 controller over Industrial Ethernet (PROFINET)?" -> Possible causes from panel images V17 Update 6: "No connection to PLC after WinCC Panel Images V17 Update 6" I hope they can be of help to you. Best regards!
|
If this Information really helps, you could use the Rate function |
|
1/2/2025 10:29 AM | |
Joined: 7/10/2024 Last visit: 9/18/2025 Posts: 180 Rating:
|
Hello Thong_Nguyen! I recommend you check the FAQs that are in the answer to the post above. I also add this one. It is usually solved since the failure of the configuration is usually described in these FAQs. - https://support.industry.siemens.com/cs/ww/en/view/69864408 I hope it helps 🍀 |
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
Follow us on