12/18/2018 2:29 PM | |
Posts: 7 Rating:
|
Dear all, kindly asking for your help. I'm trying to do the silent installation of SIMATIC WinCC flexible 2008 SP5 Standard. So what I did was to run the Setup.exe /record and went through the record procedure. At the end Ra_Auto.ini was generated. Then I moved the Ra_Auto.ini to the same folder where Setup.exe is, and run Setup.exe /silent but the installation does not start. Additionally, I put the Ra_Auto.ini in the same folder as Setup.exe and also in the folder InstData but it still didn't work. Please, advise how to do the silent installation of SIMATIC WinCC flexible 2008 SP5 Standard ? Thank you very much !!! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/19/2018 9:56:00 AMNew subject after splitting Last edited by: hrvoje.lugaric at: 12/20/2018 7:03:48 AMLast edited by: hrvoje.lugaric at: 12/20/2018 7:05:28 AM |
|
12/27/2018 10:23 AM | |
Posts: 7 Rating:
|
anyone |
Follow us on